STM32G4 Interrupt Enables I2C
Is it necessary to enable interrupts in I2C_CR1 if I only want to look at the flags but don't want to go into the interrupt service routine? For instance, I want to be able to look at the status of RXNE and see if it is set, but I don't actually want go into an interrupt routine. Can I just leave RXIE (the bit that enables the interrupt) as 0?
I am keeping RXIE as 0 for now, and I am still seeing RXNE get set when Rx data comes in. Is this normal?