Skip to main content
Visitor II
August 25, 2024
Question

STM32G4 without VSSA pin

  • August 25, 2024
  • 2 replies
  • 909 views

I'm using the STM32G431CBU3 in a project that shares the same ground for digital and analog supplies, but the UFQFPN-48 package doesn't have a VSSA pin like the others. What should I do in this situation? Should I consider VREF as my VSSA?

 

Captura de tela 2024-08-24 220819.png

    This topic has been closed for replies.

    2 replies

    Super User
    August 25, 2024

    No doubt VSS is bonded internally to VSSA/VREF-. Grounds must all be tied together, they are not independent.

    Technical Moderator
    August 25, 2024

    Dear @Liann1 ,

    VREF+ is used for the positive voltage ,  you can connect to VDDA if you do not need a precise ADC conversions .  As said by @TDK  All analog and digital grounds including VSSA are bonded at package level to a common VSS.

    Hope it helps 

    STOne-32