STM32G431 Comparator output to Timer
Hello.
STM32G431CBT6
Is it possible to route the output from the comparator to the input of the Timer input? The reference manual says that this is possible, but there is no description. And in the comparator register there are no options for choosing where to send the output.
Previously, I used stm32f072, and in the comparator settings there is an "OUTSEL" bit field where you can select where the output will be connected.
I need to measure the signal period (timer in "input capture" mode).