STM32G431 FDCAN filter doesn't work.
Hi guys.
I am using STM32G431KBT MCU. I am using 2 MCU (master / slave) and they communicate via canbus. Canbus is working good but canbus filter is not working. Master canbus address is 0x200 ans slave address is 0x101. I changing master ID (0x150) but the slave still continues to receive data and go to the canbus callback program. Cubemx settings are as follows;


And program is here;
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_ADC1_Init();
MX_FDCAN1_Init();
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
Configure_FDCAN_Filter();
if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK) {
Error_Handler();
}
if (HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK) {
Error_Handler();
}
Config_CANTX();void Configure_FDCAN_Filter(void)
{
FDCAN_FilterTypeDef sFilterConfig;
sFilterConfig.IdType = FDCAN_STANDARD_ID; // Standart 11-bit ID
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0x200; // Filtre ID
sFilterConfig.FilterID2 = 0x200; // Maske (sadece 0x200 adresini kabul et.)
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK) {
Error_Handler();
}
}void Config_CANTX(void)
{
TxHeader.Identifier = CANBUS_ID;
TxHeader.IdType = FDCAN_STANDARD_ID;
TxHeader.TxFrameType = FDCAN_DATA_FRAME;
TxHeader.DataLength = FDCAN_DLC_BYTES_8; // 8 bayt veri
TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
TxHeader.BitRateSwitch = FDCAN_BRS_OFF; // CAN FD degil, klasik CAN
TxHeader.FDFormat = FDCAN_CLASSIC_CAN;
TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
TxHeader.MessageMarker = 0;
}
I tried the every filter type (mask, dual, range) but Canbus filter is doesn't work and accepts all addresses. I am watching RxHeader in debug watch. RxHeader.Identifier is 0x00000150 and program goes to HAL_FDCAN_RxFifo0Callback with every new message. Whats is the problem?