STM32G431KB DAC DMA not working
Trying to get a basic sample DAC1 with DMA, triggered by TIM2 working.
This should be trivial, works fine on SMT32F3. I'm using a Nucleo-32 SMT32G431.
Using Cube IDE. The only non IDE-generated code in main is:
/* USER CODE BEGIN 2 */
static uint16_t x[4];
x[0]= 100;
x[1]= 1000;
x[2]= 2000;
x[3]= 3000;
HAL_TIM_Base_Start_IT(&htim2);
HAL_DAC_Start_DMA(&hdac1, DAC_CHANNEL_1, (uint32_t*)x, 4, DAC_ALIGN_12B_R);
/* USER CODE END 2 */IOC configuration:
- DAC with output buffer (verified, works fine in non-DMA mode)
- circular DMA buffer, 1/2 word
- trigger: TIM2 update
- TIM2: set to count up to 500, internal clock (works, verified by reading the clock)
Compared to some DAC/DMA examples - everything seems fine (and works on a Nucleo-32 SMT32F3. Please help - this is extremely frustrating and has held up a a project for 3 days.
test1.ioc and main.c files attached.
Thank you!
Paul