STM32G47 PA9 Appears to be Set high in bootloader mode opposed to pulled high
As the title says, the STM32G47 PA9 pin appears to be set high in boot mode opposed to pulled high though a resistor which is states in AN2606. This is becoming a problem because it introduces negative behaviors in our design when we try to reprogram. Is this a known behavior documented elsewhere?
I have gotten pretty frustrated when migrating from the STMF3 family to the STMG4 since there are many more pins being pulled or set in one direction or another during boot mode.
Is there any way to disable some of these hardware defined communications protocols during the boot loader mode initiated by the BOOT0 pin?