Question
STM32G474 boot
Hi, I have a STM32G474 connected to a Quectel LTE module via a uart4 and a GPIO pin.
Under normal conditions is it possible for the CPU to boot from flash and when the quectel changes the level of the gpio pin of the STm32, the CPU jump to boot from uart4 to update the firmware?
Is this the best solution, using a GPIO pin?
Many Thanks.