STM32G474CEU6 with 1.8V supply
Hi, The STM32G474CEU6 LQFPN48 was previously used in our projects with a 3.3 V supply, where we successfully operated a 25 MHz FL2500326 crystal using 6.8 pF load capacitors, and the crystal oscillation was stable.
In the current design, the same controller is powered at 1.8 V for all VDD, VDDA, and VREF+ pins, while using the same crystal and the same load capacitors. However, under this configuration, the crystal oscillator does not start, and no crystal output is observed.
As an alternative, we are currently using HSI clock (16 MHz) as system clock in our application. It is observed in other posts that HSI cannot be used for high speed peripherals like USB and Ethernet due to it's low accuracy, and also it varies with temperature. In our application, we are using 2 - UARTs, 2 - I2Cs and one SPI along with few GPIOs.
Is it recommendable to run the STM32g474 with 1.8V VDD? Also can someone give advice on the HSI system clock mode?
Please let us know how to solve this issue.