STM32G474RET Linker Question
In the linker script provided by STM for STM32G474RETx, the memory section is:
MEMORY
{
CCMSRAM (xrw) : ORIGIN = 0x10000000, LENGTH = 32K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 512K
}But in the reference manual RM0440 section 2.4 page 88 it states that:
Category 3 devices feature up to 128 Kbytes SRAM:
• 80 Kbytes SRAM1 (mapped at address 0x2000 0000)
• 16 Kbytes SRAM2 (mapped at address 0x2001 4000)
• 32 Kbytes CCM SRAM (mapped at address 0x1000 0000 and end of SRAM2)
I'm confused as to why the RAM is declared as 128K when that's the combined total of SRAM1 + SRAM2 + CCMSRAM, and there's also CCNSRAM declared separately. Is it so that RAM covers all SRAM but you can also place specific things in the CCMSRAM section?