STM32G491RE QUADSPI ISSUE
Hello,
I'm facing a strange issue with the quadspi peripheral.
I'm using it to interface with a W25q256jveiq, a quad spi enabled flash chip from Winbond.
As long as I use one line SPI or dual I/O mode all works fine.
I can access the flash chip with no issue at a 80 MHz clock speed.
As soon as I switch to a quad I/O mode I'm facing a strange issue.
A string signature is stored at address 0.
The written signature is correct, I can read it properly in dual I/O mode.
In quaq I/O modes the \r\n bytes in the string are not read properly but all other characters are.properly read.
The alternate byte is properly set (it works fine in dual I/O mode).
The dummy clock cycles are set according to the data sheet (may be I'm wrong about them, the main difference with dual I/O mode is that there's no dummy clock cycles in dual I/O mode).
The command for dual I/O mode is:
com.InstructionMode = QSPI_INSTRUCTION_1_LINE;
com.Instruction = 0xBC; // Fast Read Dual I/O with 4-Byte Address
com.AddressSize = QSPI_ADDRESS_32_BITS;
com.AddressMode = QSPI_ADDRESS_2_LINES;
com.Address = buffer_address;
com.AlternateByteMode = QSPI_ALTERNATE_BYTES_2_LINES;
com.AlternateBytes = 0xFF;
com.AlternateBytesSize = QSPI_ALTERNATE_BYTES_8_BITS;
com.DummyCycles = 0;
com.DataMode = QSPI_DATA_2_LINES;
com.NbData = data_length;
com.DdrMode = QSPI_DDR_MODE_DISABLE;
com.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
com.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
The command setup for quad I/O is:
com.InstructionMode = QSPI_INSTRUCTION_1_LINE;
com.Instruction = 0xEC; // Fast Read Quad I/O with 4-Byte Address
com.AddressSize = QSPI_ADDRESS_32_BITS;
com.AddressMode = QSPI_ADDRESS_4_LINES;
com.Address = buffer_address;
com.AlternateByteMode = QSPI_ALTERNATE_BYTES_4_LINES;
com.AlternateBytes = 0xFF;
com.AlternateBytesSize = QSPI_ALTERNATE_BYTES_8_BITS;
com.DummyCycles = 4;
com.DataMode = QSPI_DATA_4_LINES;
com.NbData = data_length;
com.DdrMode = QSPI_DDR_MODE_DISABLE;
com.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
com.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
To be sure that the issue is not related to the data length, I've inserted a \r\n pair in the middle of the string and they are also corrupted with the same data pattern as the ending \r\n.
I've tried another command, 0x6C (Fast Read Quad Output with 4-Byte Address [address is sent in 1 line mode],), same issue despite the fact that this command does not require the alternate byte but 8 dummy clock cycles instead of 4 for the 0xEC command.
Look at the differences in locations [55], [56] and [57]
Data read in QUAD I/O Mode
flash_page_bufferuint8_t [64]0x20003098 <ucHeap+6584>
flash_page_buffer[0]uint8_t83 'S'
flash_page_buffer[1]uint8_t84 'T'
flash_page_buffer[2]uint8_t77 'M'
flash_page_buffer[3]uint8_t51 '3'
flash_page_buffer[4]uint8_t50 '2'
flash_page_buffer[5]uint8_t71 'G'
flash_page_buffer[6]uint8_t52 '4'
flash_page_buffer[7]uint8_t57 '9'
flash_page_buffer[8]uint8_t49 '1'
flash_page_buffer[9]uint8_t86 'V'
flash_page_buffer[10]uint8_t69 'E'
flash_page_buffer[11]uint8_t84 'T'
flash_page_buffer[12]uint8_t32 ' '
flash_page_buffer[13]uint8_t87 'W'
flash_page_buffer[14]uint8_t101 'e'
flash_page_buffer[15]uint8_t97 'a'
flash_page_buffer[16]uint8_t116 't'
flash_page_buffer[17]uint8_t104 'h'
flash_page_buffer[18]uint8_t101 'e'
flash_page_buffer[19]uint8_t114 'r'
flash_page_buffer[20]uint8_t32 ' '
flash_page_buffer[21]uint8_t83 'S'
flash_page_buffer[22]uint8_t116 't'
flash_page_buffer[23]uint8_t97 'a'
flash_page_buffer[24]uint8_t116 't'
flash_page_buffer[25]uint8_t105 'i'
flash_page_buffer[26]uint8_t111 'o'
flash_page_buffer[27]uint8_t110 'n'
flash_page_buffer[28]uint8_t32 ' '
flash_page_buffer[29]uint8_t40 '('
flash_page_buffer[30]uint8_t67 'C'
flash_page_buffer[31]uint8_t41 ')'
flash_page_buffer[32]uint8_t32 ' '
flash_page_buffer[33]uint8_t50 '2'
flash_page_buffer[34]uint8_t48 '0'
flash_page_buffer[35]uint8_t50 '2'
flash_page_buffer[36]uint8_t52 '4'
flash_page_buffer[37]uint8_t32 ' '
flash_page_buffer[38]uint8_t77 'M'
flash_page_buffer[39]uint8_t83 'S'
flash_page_buffer[40]uint8_t111 'o'
flash_page_buffer[41]uint8_t102 'f'
flash_page_buffer[42]uint8_t116 't'
flash_page_buffer[43]uint8_t32 ' '
flash_page_buffer[44]uint8_t82 'R'
flash_page_buffer[45]uint8_t101 'e'
flash_page_buffer[46]uint8_t118 'v'
flash_page_buffer[47]uint8_t46 '.'
flash_page_buffer[48]uint8_t32 ' '
flash_page_buffer[49]uint8_t48 '0'
flash_page_buffer[50]uint8_t46 '.'
flash_page_buffer[51]uint8_t48 '0'
flash_page_buffer[52]uint8_t46 '.'
flash_page_buffer[53]uint8_t48 '0'
flash_page_buffer[54]uint8_t99 'c'
flash_page_buffer[55]uint8_t0 '\0'
flash_page_buffer[56]uint8_t160 ' '
flash_page_buffer[57]uint8_t15 '\017'
flash_page_buffer[58]uint8_t255 'ÿ'
flash_page_buffer[59]uint8_t255 'ÿ'
flash_page_buffer[60]uint8_t255 'ÿ'
flash_page_buffer[61]uint8_t255 'ÿ'
flash_page_buffer[62]uint8_t255 'ÿ'
flash_page_buffer[63]uint8_t255 'ÿ'
Data read in DUAL I/O Mode
flash_page_bufferuint8_t [64]0x20003098 <ucHeap+6584>
flash_page_buffer[0]uint8_t83 'S'
flash_page_buffer[1]uint8_t84 'T'
flash_page_buffer[2]uint8_t77 'M'
flash_page_buffer[3]uint8_t51 '3'
flash_page_buffer[4]uint8_t50 '2'
flash_page_buffer[5]uint8_t71 'G'
flash_page_buffer[6]uint8_t52 '4'
flash_page_buffer[7]uint8_t57 '9'
flash_page_buffer[8]uint8_t49 '1'
flash_page_buffer[9]uint8_t86 'V'
flash_page_buffer[10]uint8_t69 'E'
flash_page_buffer[11]uint8_t84 'T'
flash_page_buffer[12]uint8_t32 ' '
flash_page_buffer[13]uint8_t87 'W'
flash_page_buffer[14]uint8_t101 'e'
flash_page_buffer[15]uint8_t97 'a'
flash_page_buffer[16]uint8_t116 't'
flash_page_buffer[17]uint8_t104 'h'
flash_page_buffer[18]uint8_t101 'e'
flash_page_buffer[19]uint8_t114 'r'
flash_page_buffer[20]uint8_t32 ' '
flash_page_buffer[21]uint8_t83 'S'
flash_page_buffer[22]uint8_t116 't'
flash_page_buffer[23]uint8_t97 'a'
flash_page_buffer[24]uint8_t116 't'
flash_page_buffer[25]uint8_t105 'i'
flash_page_buffer[26]uint8_t111 'o'
flash_page_buffer[27]uint8_t110 'n'
flash_page_buffer[28]uint8_t32 ' '
flash_page_buffer[29]uint8_t40 '('
flash_page_buffer[30]uint8_t67 'C'
flash_page_buffer[31]uint8_t41 ')'
flash_page_buffer[32]uint8_t32 ' '
flash_page_buffer[33]uint8_t50 '2'
flash_page_buffer[34]uint8_t48 '0'
flash_page_buffer[35]uint8_t50 '2'
flash_page_buffer[36]uint8_t52 '4'
flash_page_buffer[37]uint8_t32 ' '
flash_page_buffer[38]uint8_t77 'M'
flash_page_buffer[39]uint8_t83 'S'
flash_page_buffer[40]uint8_t111 'o'
flash_page_buffer[41]uint8_t102 'f'
flash_page_buffer[42]uint8_t116 't'
flash_page_buffer[43]uint8_t32 ' '
flash_page_buffer[44]uint8_t82 'R'
flash_page_buffer[45]uint8_t101 'e'
flash_page_buffer[46]uint8_t118 'v'
flash_page_buffer[47]uint8_t46 '.'
flash_page_buffer[48]uint8_t32 ' '
flash_page_buffer[49]uint8_t48 '0'
flash_page_buffer[50]uint8_t46 '.'
flash_page_buffer[51]uint8_t48 '0'
flash_page_buffer[52]uint8_t46 '.'
flash_page_buffer[53]uint8_t48 '0'
flash_page_buffer[54]uint8_t99 'c'
flash_page_buffer[55]uint8_t13 '\r'
flash_page_buffer[56]uint8_t10 '\n'
flash_page_buffer[57]uint8_t0 '\0'
flash_page_buffer[58]uint8_t255 'ÿ'
flash_page_buffer[59]uint8_t255 'ÿ'
flash_page_buffer[60]uint8_t255 'ÿ'
flash_page_buffer[61]uint8_t255 'ÿ'
flash_page_buffer[62]uint8_t255 'ÿ'
flash_page_buffer[63]uint8_t255 'ÿ'
Thanks in advance