STM32H5 getUID with enabled ICACHE
Hi.
Is there any consideration that I need to take care of when I use HAL_GetUIDw0~2 while ICACHE is enabled?
even the simplest project with STM32H573IIK3Q that the ICACHE is enabled will get a hardfault when trying to get UID bytes.
This is the whole code that I have:
/* USER CODE BEGIN WHILE */
while (1)
{
uint32_t x,y,z;
x=HAL_GetUIDw0();
//y=HAL_GetUIDw1();
//z=HAL_GetUIDw2();
HAL_Delay(1000);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */