STM32H5 high-cycle data read more than 16bit at once
Hi,
I'm using STM32H563 and managed to set FLASH_EDATA1R_CUR as needed (EDATA1_EN="1", EDATA1_STRT="111"). Then I tried to read 64-Bit at once from Address 0x09000000. Unfortunately I get a hard fault. Is it intended to read more than 16 bit from the high cycle memory?
Even with the debugger and Cube IDE 1.13.0 I have problems accessing the memory from high cycle data. It keeps saying, that the memory content cannot be obtained.
Please give advice how to work with the high cycle data!
Thanks,
Johannes