STM32H5 Interface With Gigabit Ethernet PHY device
Moved from MPUs forum.
Hi, i must Use a Single Port Gigabit Ethernet PHY that have a RGMII Gigabit Interface to connect a RMII 10/100 Mbit
Ethernet MAC interface of the STM32H563VI MCU.
Do you think it is possible to connect a Gigabit PHY chip to the 100 Mbit H5 micros??? pin out,
Sure the final Ethernet Speed of the system, will be declasses to 10/100 Mbit.
In particular I can't find where to connect the PA7 pin [RMII_CRS_DV] Carrier Sense... there is no CRS_DV output in the PHY gigabit device
Thank you very much