Skip to main content
Visitor II
May 28, 2025
Question

STM32H503 code execution performance issue

  • May 28, 2025
  • 2 replies
  • 978 views

Hello

for some specific usage I am evaluating possibilities of using CM33 with HCLK 250MHz for maximum code execution performance. 

To do so I have crafted procedure in assembler and calculated the cycles using ARM reference manual. The code is doing only some data conversation from one data buffer into another one. 

Then I place this code in SRAM1, enabling I-Cache, setting RCC and I try to measure code execution time. 

Let’s say execution cycles calculated by hand is about 3000. 

later work I am basing on the code generated by CubeMX and inject my bare metal stuff. 

1) using DWT->CYCCNT I see no difference in execution from FLASH or SRAM1 - result is about 7900
2) using TIM6 started before my func and stopped after it thus TIM->CNT has time in 4ns intervals - formal cycles. Running from SRAM -same result. 

 

Example of the „issue” 

LDR r0, =label

 

During step debugging for this instruction the TIM6->CNT is incremented by 6 units. 

 

Same for 

TST r0, #1

6 units of CNT change thus 6 cycles. 6x slower than it should be executed. 

My question is: 

Is the STM32H5 value line prepared in the way that peripherals can but cpu core ca not work with 250MHz HCLK?

Or I am not initializing this CPU properly so with HCLK 250MHz I am achieving similar code performance as with G0 at 48MHz?

I feel I am missing something…

    This topic has been closed for replies.

    2 replies

    Visitor II
    May 29, 2025

    I couldn't even get this stm32h503 chip to work. After 10 minutes of working, the reset pin goes to low and it doesn't work anymore. We think this product is completely faulty. Were you able to get it to work? Which product are you using exactly?

    Graduate II
    May 29, 2025

    >>We think this product is completely faulty.

    I'd wager it's a problem on your end

    Visitor II
    May 29, 2025

    If you know of a problem that will cause the product to burn and break, I am open to any help.

    şema.png

    Super User
    May 29, 2025

    What optimizer setting you have ? (without ...no fun. :) )

    +

    You cannot debug ONE instruction , to see its timing.

     

    btw

    I tried on a H563 , at 250M core clock, and it works at 4ns cycles - as it should.

    I checked just by writing to a pin in a loop ...and check with scope.

    Visitor II
    May 29, 2025

    Typical STM32CubeIDE settings. 
    I tried to run my code from flash and RAM (albeit I have not managed to put only that function there using RamFunc - trampoline code added by linker did not work, thumb bit not set this hardfault all the time. But when I have put all my code in the RAM - that worked)

     

    yes i learned that I can not debug single instruction. When I plugged toggling of the GPIO and hooked up the scope - measurement was close to the theoretical calculations. 

    the same result I have when I placed the measurement (dwt or tim) to the table that I monitor as live view. And run the code without any breakpoints.  

    Super User
    May 29, 2025

    >Typical STM32CubeIDE settings. 

    What are these "Typical" settings, regarding the optimizer setting ?