Skip to main content
Visitor II
May 29, 2025
Question

STM32H503CBT6 NRST and VCAP Behavior – Severe Stability Issue

  • May 29, 2025
  • 1 reply
  • 469 views

Hello,

I’m using the STM32H503CBT6 microcontroller in my project. At this stage, the firmware simply toggles a single LED. I’m using STM32CubeMX (code configurator) and compiling with STM32CubeIDE. The system is configured to run at 250 MHz using a 16 MHz HSE with the PLL, according to the recommendations in the documentation.

Hardware Configuration:

NRST pin is pulled up to 3.3V with a 4.7k resistor and has a 100nF capacitor to GND.

BOOT0 is pulled down to GND with a 10k resistor.

Both VCAP pins have 2.2µF ceramic capacitors.

All unused GPIOs are left in floating mode via CubeMX configuration.

VDD is supplied with a stable 3.3V.

Observed Issues:

The system enters a fault state randomly, between 10 seconds and 10 minutes after power-up.

In the fault state:

VDD remains at 3.3V.

NRST pin oscillates between ~0.5V and ~0.9V.

VCAP voltage drops to around 1V (where it should normally be ~1.36V).

Before entering the fault state, NRST sometimes fluctuates between 3.3V and 2V for a short while.

After the fault, the microcontroller becomes permanently non-functional. It starts drawing excessive current and does not recover.

So far, we’ve damaged around 20 STM32H503CBT6 chips across different PCBs.

Power has been supplied from different sources:

USB port of a computer,

Regulated lab power supply,

3.3V battery source.
The same issue occurs with all power setups.

Best regards.

    This topic has been closed for replies.

    1 reply

    Super User
    May 29, 2025

    This indicates a hardware issue. Perhaps show the full schematic. Ensure pins are not being overvoltaged.

    > So far, we’ve damaged around 20 STM32H503CBT6 chips across different PCBs.

    Probably a critical flaw in the design then, yes?

     

    There are no issues with your BOOT0/NRST/VCAP setups.

    kadir1Author
    Visitor II
    May 29, 2025

    şema.png

    Theoretically, there should be no problem with the scheme.

    Super User
    May 29, 2025

    How does one net have two different names? +3V3 and +3V3_MCU are connected. What are E3 and Z3 here?

    Hard to debug through a keyhole. No obvious issues with what you posted but there's certainly an issue somewhere. If you don't want to post the schematic, all I can offer are general tips.

    Getting started with STM32H5 MCU hardware development - Application note