stm32H503RB Determination of I3C IBI payload size
Hi,
I am using the nucleo-H503RB I3C (Controller mode) with this example to connect to an I3C standard chip. The sensor transmits IBI with 5 bits of payload but I noticed that the STM32 receives only 4 bits, and then it stops receiving the fifth bit.
Is there any method I can define the receive IBI payload size on the controller side? Any kind of help is appreciated. :)