STM32H503RB I3C private communication
Hi all,
I tried to communicate(private) with my I3C slave device by using STM32H503RB board (as a controller).
Here's the code from "Introduction to I3C for STM32 MCUs - Application note Chapter 9.8 Private read"
uint8_t aTxBuffer[1] = {0x0F};
uint8_t aRxBuffer[1];
TargetDesc_TypeDef *aTargetDesc[1] = \
{
&TargetDesc1, /* DEVICE_ID1 */
};
/* Descriptor for private data transmit */
I3C_PrivateTypeDef aPrivateDescriptor[2] = \
{
{TARGET1_DYN_ADDR, {aTxBuffer, TXBUFFERSIZE}, {NULL, 0}, HAL_I3C_DIRECTION_WRITE},
{TARGET1_DYN_ADDR, {NULL, 0}, {aRxBuffer, RXBUFFERSIZE}, HAL_I3C_DIRECTION_READ}
};
aContextBuffers[I3C_IDX_FRAME_1].CtrlBuf.pBuffer = aControlBuffer;
aContextBuffers[I3C_IDX_FRAME_1].CtrlBuf.Size = 1;
aContextBuffers[I3C_IDX_FRAME_1].TxBuf.pBuffer = aTxBuffer;
aContextBuffers[I3C_IDX_FRAME_1].TxBuf.Size = TXBUFFERSIZE;
/* Prepare Receive context buffer with the different parameters */
aContextBuffers[I3C_IDX_FRAME_2].CtrlBuf.pBuffer = aControlBuffer;
aContextBuffers[I3C_IDX_FRAME_2].CtrlBuf.Size = 1;
aContextBuffers[I3C_IDX_FRAME_2].RxBuf.pBuffer = aRxBuffer;
aContextBuffers[I3C_IDX_FRAME_2].RxBuf.Size = RXBUFFERSIZE;
if (HAL_I3C_AddDescToFrame(&hi3c1,
NULL,
&aPrivateDescriptor[I3C_IDX_FRAME_1],
&aContextBuffers[I3C_IDX_FRAME_1],
aContextBuffers[I3C_IDX_FRAME_1].CtrlBuf.Size,
I3C_PRIVATE_WITH_ARB_RESTART) != HAL_OK)
{
/* Error_Handler() function is called when error occurs. */
Error_Handler();
}
if (HAL_I3C_Ctrl_Transmit_IT(&hi3c1, &aContextBuffers[I3C_IDX_FRAME_1]) != HAL_OK)
{
/* Error_Handler() function is called when error occurs. */
Error_Handler();
}
while (HAL_I3C_GetState(&hi3c1) != HAL_I3C_STATE_READY)
{
}
if (HAL_I3C_AddDescToFrame(&hi3c1,
NULL,
&aPrivateDescriptor[I3C_IDX_FRAME_2],
&aContextBuffers[I3C_IDX_FRAME_2],
aContextBuffers[I3C_IDX_FRAME_2].CtrlBuf.Size,
I3C_PRIVATE_WITH_ARB_STOP) != HAL_OK)
{
/* Error_Handler() function is called when error occurs. */
Error_Handler();
}
if (HAL_I3C_Ctrl_Transmit_IT(&hi3c1, &aContextBuffers[I3C_IDX_FRAME_2]) != HAL_OK)
{
/* Error_Handler() function is called when error occurs. */
Error_Handler();
}
}
After running debug, the error occurs in "static HAL_StatusTypeDef I3C_Xfer_PriorPreparation()"
condition (global_tx_size > hi3c->pXferData->TxBuf.Size) will always be satisfied unless 'aTxBuffer[]' has more than 147 elements.
Did anyone encounter this problem before?
Btw, should I execute ENTDAA before PrivateRead?