STM32H533 DCACHE seems to make no difference?
So I've got a program with a fast tight loop doing some minimal things, and the rest is housekeeping/UI stuff in the main loop. When I enabled ICACHE, the speed of the tight loop increased DRAMATICALLY and overall the process is faster at basically everything. A colleague of mine said that he uses the DCACHE also and that for his application on an H7, the DCACHE made a huge performance improvement. But, as far as I can measure (which is toggling GPIO pins at critical sections of code and measuring the time with o-scope), the DCACHE made no difference on or off.
So for now I 'm just leaving it off because I know I need to be careful with DCACHE and my SD Card etc. and it's easier to just leave it off, but I'm wondering what areas/use cases is the DCACHE actually supposed to improve with this chip?