STM32H562 - 5V Tolerant Pins Derating Impact
Hello Community,
We are currently evaluating the STM32H562IGT6 microcontroller for our development project. During our review of the device’s pinout, we observed that several GPIO pins are designated as FT (5‑V tolerant). We would like to request clarification regarding the electrical behavior and long‑term reliability of these pins when subjected to a continuous 5 V digital input.
Specifically, we would like to understand whether applying a constant 5 V signal to the FT‑labeled pins may have any impact on product lifetime, derating considerations, or long‑term performance degradation.
The following pins are of particular interest for this inquiry:
| PC0 | FT_a |
| PC1 | FT_ah |
| PA0 | FT_at |
| PA6 | FT_ah |
| PA7 | FT_ah |
| PC4 | FT_a |
| PC5 | FT_ah |
| PB1 | FT_ah |
Thank you.
Regards,
Rajesh Matere