STM32H563 clock at 250Mhz
I was trying to get the most out of my H563 set up and run as fast as possible.
I am using the Nucleo-H563 board.
I reconfigured in CubeMX to use System clock mux to use HSE source mux, multipliers and dividers set correctly for 250MHZ operation. There are no errors shown in the setup and I am showing 250 Mhz as the SYSCLK. My AHB is /1, HCLK shows 250MHZ which is feeding the peripheral busses.
While the clock configuration APB1 shows 250Mhz it does not seem to be correct as when I set the timers and prescalers for such the timing is not correct... the bus seems to be running at 125mhz.
For my TMR1 to get 1us clock I have to set the divider to 124 which implies the internal clock is running at 125Mhz not 250 like the clock diagram shows.
I have attached the Clock Configuration from CubeMX that shows no clock issues.