STM32H563 SPI DMA issue
Hi All!
I have a issue about SPI DMA communication on NUCLEO-H563 Board. Details are as follows.
My Configuration of STM32CubeMx as shown in the figure1 and 2.

figure1

figure2
I call the function of HAL_SPI_TransmitReceive_DMA(), it comes to line 2212 of program and return HAL_ERROR then.
I debug the program and find the value of hspi->hdmarx->Init.DestDataWidth is 0, so it return the error.
Then I back to check the initialization of spi1 dma. I find that the Init.DestDataWidth of handle_GPDMA1_Channel2 is already 0 before execute statement __HAL_LINKDMA() .
So I guess maybe somewhere my configuration of spi dma is wrong somewhere and I can't figure it out.
Please help me for this question.
Thanks!