STM32H573 CUSTOM BOARD VCAP PIN NOT OUTPUTING VOLTAGE
I have designed a custom board using STM32H573IIT3Q MCU. when I connected it with st link, the st link not recognize it. After I check the voltage on power pin, all the power pin is normal except the VCAP pin (not outputing voltage). According to the AN5711, I am using the LDO configuration and here is the schematic of MCU's power.
the BOOT pin pulled down with 10K resistor, and the reset pin is on high state when the board powered.
I have tried bypass the vcap pin with buck and the board is connected with st link and haven't found any problem but I want to use the internal LDO configuration. does someone knows what the issue is ? thank you