STM32H573V UCPD CC2 and PC9 interference
HI,
I am working on a board using STM32H573V and have a working solution with UCPD detecting an inserted memory stick and running the MSC class. In an other part of the software I am using PC9 as an GPIO push-pull, low speed output and as soon as I set it to high, the voltage at PB14 (UCPD CC2) drops from 3.3V to 1.5V and my UCPD handler signals a device attached and turns VBUS on even though nothing is attached. There is no other electrical connection between PC9 and PB14 on the board. I am using a TCPP03-M20 for VBUS switching. The board is acting as VBUS source.