Skip to main content
Explorer
July 22, 2024
Question

STM32H7 ADC faster than expected

  • July 22, 2024
  • 3 replies
  • 2228 views

Hello,

Using a STM32H743ZI - rev. V.

I'm using ADC3 to convert 4 channels in regular conversion mode, with a 2.5Tcy sampling time, 10 bits, sync clock /2.

The measured conversion time is quicker than expected so I'm suspecting something wrong...

CPU clock is 400MHz, AXI/AHB clock is 100MHz.

DMA transfers ADC results to AXI SRAM. I've fine tune my program for speed (gcc optimization for speed, release mode, interrupt routine relocated in ITCM with only the necessary code). 

TIM15 trigs the ADC, and also activate an output pin.

The first thing I do in the DMA interrupt is to rise a GPIO pin. So, I can measure the total time : TRIG + sampling & conversion + DMA transfert time + IRQ latency + GPIO write.

This measured time is 1100ns.

The ADC clock is 100MHz divided by 2 (CKMODE=0b10) and by 2 (internal /2 in rev V version) so 25MHz <=> Tck=40ns.

Trig time : 1.5~2.5Tck

Samp time : 4*2.5Tcy = 10Tck

Conv time : 4*(N/2+0.5) = 22Tck

Total expected time : 33.5~34.5Tck = 1340~1380ns => 23% faster than measured. There is definitely something wrong in my configuration or interpretation.

Many thanks pour your help :)

ADC config:

 

 hadc3.Instance = ADC3;
 hadc3.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
 hadc3.Init.Resolution = ADC_RESOLUTION_10B;
 hadc3.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc3.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc3.Init.LowPowerAutoWait = DISABLE;
 hadc3.Init.ContinuousConvMode = DISABLE;
 hadc3.Init.NbrOfConversion = 4;
 hadc3.Init.DiscontinuousConvMode = DISABLE;
 hadc3.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T15_TRGO;
 hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc3.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
 hadc3.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 hadc3.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
 hadc3.Init.OversamplingMode = DISABLE;

 

 

Clock config with 20MHz crystal:

 

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 2;
 RCC_OscInitStruct.PLL.PLLN = 80;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }

 

 

    This topic has been closed for replies.

    3 replies

    Super User
    July 22, 2024

    Conversion and DMA may overlap?

     

     

    Super User
    July 22, 2024

    Hi,

    so Tck (25M->40ns) is the ADC clock - right ? 

    ADC needs at N=10 bits + 2.5 sampling:  2.5 + (N/2+0.5) = 8 x 40ns = 320ns ( 3Msps )

    So some delay in your measurement, if you see 1100ns.

    >23% faster than measured

    How you measure it ?

    tarzan2Author
    Explorer
    July 23, 2024

    @AScha.3 wrote:

    so Tck (25M->40ns) is the ADC clock - right ? 

    ADC needs at N=10 bits + 2.5 sampling:  2.5 + (N/2+0.5) = 8 x 40ns = 320ns ( 3Msps )

    So some delay in your measurement, if you see 1100ns.

    >23% faster than measured

    How you measure it ?


    There is 4 channels in regular conversion mode. So 320ns*4=1280ns.

    Adding trigger time, DMA transfert time, IRQ latency and GPIO write, I would expect to measure something between 1400 and 1600ns, I dont know... But definitely it should be more than 1280ns !

    I could think that the ADC clock is not 25MHz but faster, making the sampling time and boost bits wrong.

    I measure it with a 1GS/s scope :

    - Channel 1 on TIM15 output, showing the beginning of ADC conversion

    - Channel 2 on a GPIO rised at the beginning of the DMA interrupt :

    void DMA2_Stream3_IRQHandler(void) // @ITCM RAM
    {
     GPO_TP3_GPIO_Port->BSRR = GPO_TP3_Pin;
     asm volatile("" ::: "memory"); // Avoid asm code re-ordering by the optimizer.

     

    tarzan2Author
    Explorer
    July 23, 2024

    Some news...

    - In debug mode, all ADC registers, including clocks and sampling time, are good.

    - The MCO configured to output SYSCLK/10 is toggling at 40MHz. So SYSCLK is verified at 400MHz.

    Modifying the ADC sampling time give some interesting results. It looks like the ADC clock is 50MHz instead of 25MHz. 

    Looking more carefully how the ADC clock sclk is generated, I've found it is derived from sys_clk, not from ahb_clk. My adc was actually clocked at 50MHz. After reprogramming CKMODE to /4 instead of /2, the timings are looking ok.

    The datasheet mentions the maximum adc frequency without precision about which clock we are talking about. I assume it is the final conversion clock. There is nothing about potential limitation on adc_sclk and adc_hclk. I assume they can accept all sysclk and ahbclk range.

    A more unfortunate thing is that after reading AN5354, I see that the ADC clock is also limited by the package. Using 3 ADC, for my LQFP144 the max clock is 30MHz and not 50MHz as specified in the datasheet. Very bad that the datasheet don't mention anything about that.

     

    Super User
    July 22, 2024

    It's difficult to measure the ADC conversion time in this way. Your measurement will include errors that aren't associated with the ADC.

    If you want to measure it, here's a good method:

    • Set up a circular ADC DMA transfer to a large buffer. Something like 1000 samples.
    • Within the transfer complete callback, toggle a pin.
    • Measure the time between two successive toggles to estimate the time it takes to capture the entire buffer.

    This method will have the same amount of overhead/delay on each toggle and will therefore cancel it out.