STM32H7 and USB-C Schematics
Hello everyone!
I'm close to validating all my schematics for a PCB project, and I wanted to be sure at 100% that a section is correct.
I'm talink about the USB-C section, that connects directly to the STM32H7 microcontroller.

It will be used to access a NAND Flash Memory that is connected via SDMMC 4 Bits Wide Bus directly to the STM32 :

Can you please tell me if there's an error?
I also saw that in some designs they connect the CC1 and CC2 pins to a 5.1k resistor each, do I have to do the same for this design?
I'm also confused about the 22 Ohms termination resistors. I saw countless forums and discussions where some people say they're necessary and other people say they're not. What's the recommendation for an STM32H7A3VIT6 microcontroller (Full Speed 12.2Mbps)?