STM32H7 Camera Buffer YUV TVP5150 JPEG
Hello
Let's assume I have a TVP5150 device connected to a STM32H7 MCU. The TVP5150 transmits PAL frames as YUV. This means 2 bytes per pixel.
This results in 720x576 * 2 = 829.440KB per frame. In reality, there is pretty sure the need for double buffering. So I guess I need ~1.65MB to store/cache frames.
There is SDRAM Support for STM32H7 allowing to connect e.g. a 64Mbit SDRAM.
Is this a "supported" setup? Can I use DMA to transfer data of the TVP5150/Camera Interface into SDRAM? Will the SDRAM and STM32H7 be fast enough for such kind of operation?
The STM32H7 should also be able to encode these frames into JPEG/MJPEG.