[STM32H7] CORTEX_M7 configuration for MPU in CUBEMX
Dear Experts,
I am looking at configuring the CORTEX_M7 section for my custom STM32H743VIT6 based board. Below are the functionalities that I plan to use with the board:
a. Sensors' reading via SPI, I2C,
b. Communication via UART/USART, USB, Ethernet (LAN8742),
c. LwIP and potentially FreeRTOS
I would like to have your advice on the disabling / enabling of caches and especially the MPU configuration/settings in case :
1. Without external QSPI Flash and external PSRAM,
2. With external QSPI Flash and/or external PSRAM
I took some look at the STM32H7-LwIP-Examples for the NUCLEO-STM32H743 board and the following h7_lwip_freertos example but there's certain different in terms of number of MPU regions being used as well as their base addresses, sizes and permissions, etc.
Where can I find the information or documentation to correctly configure the above section, please ?
Thanks in advance and best regards,
Khang