STM32H7 Custom Project prototype , power issues
Hi there,
this is my first post here. So be gentle with me ;)
I been working on a project with STM32H757XIH6 for some time now, but without any success. This is already my 2nd prototype and costed me quite some $$ since it had to be a 8 layer PCB. The soldering I have performed my self with a heat gun and heating platform...This worked fine in the past.
I checked everything already several times, but since I am doing this one alone, I most have missed something.
The issue has to be from the MCU connection/Layout since this one gets super hot when I power the board. If I desolder the MCU out, I can control the other devices(power supplies I2C devices, SPI, etc ).
The power input looks like this:

From the System supply configurations I intend to use this one (in red). Being SMPS off and Vreg on.

Am I missing something ?The 3.3V are stable when I desolder the MCU.
I would appreciate any help since I am quite stuck on this issue alone .
Much appreciated in advance.