STM32H7 DMA issue
Hello
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* htim_base)
{
if(htim_base->Instance==TIM1)
{
/* USER CODE BEGIN TIM1_MspInit 0 */
/* USER CODE END TIM1_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_TIM1_CLK_ENABLE();
/* TIM1 DMA Init */
/* TIM1_TRIG Init */
hdma_tim1_trig.Instance = DMA1_Stream1;
hdma_tim1_trig.Init.Request = DMA_REQUEST_TIM1_TRIG;
hdma_tim1_trig.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_tim1_trig.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_tim1_trig.Init.MemInc = DMA_MINC_ENABLE;
hdma_tim1_trig.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_tim1_trig.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_tim1_trig.Init.Mode = DMA_CIRCULAR;
hdma_tim1_trig.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_tim1_trig.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_tim1_trig) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_TRIGGER],hdma_tim1_trig);
/* USER CODE BEGIN TIM1_MspInit 1 */
/* 手动配置TIM1 CCR的DMA流 */
hdma_tim1_ccr.Instance = DMA1_Stream2;
hdma_tim1_ccr.Init.Request = DMA_REQUEST_TIM1_TRIG;
hdma_tim1_ccr.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_tim1_ccr.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_tim1_ccr.Init.MemInc = DMA_MINC_ENABLE;
hdma_tim1_ccr.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_tim1_ccr.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_tim1_ccr.Init.Mode = DMA_CIRCULAR;
hdma_tim1_ccr.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_tim1_ccr.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_tim1_ccr) != HAL_OK)
{
Error_Handler();
}
// 使能TIM3的触发DMA请求
TIM3->DIER |= TIM_DIER_TDE;
__HAL_LINKDMA(htim_base, hdma[TIM_DMA_ID_TRIGGER], hdma_tim1_ccr);
/* USER CODE END TIM1_MspInit 1 */
}
I use TIM3 as the master timer and TIM1 as the slave timer, with TIM3 triggering DMA.
Can the STM32H7 trigger two DMAs simultaneously with one event? I see that in STM32CubeIDE, it's one-to-one by default. Is it possible to manually add two DMA streams to modify ARR and CCR simultaneously?