STM32H7 Dual Core MCU CM4 FLASH 0x081E0000
Hello ,
I am working with stm32h747.
M4 .ld File
FLASH (rx) : ORIGIN = 0x08100000, LENGTH = 1024K
M7 .ld File
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K
With the above settings I can run Core M7 and M4 properly.
I need more flash on the m7 side and I want to separate the flash as follows
M4 .ld File
FLASH (rx) : ORIGIN = 0x081E0000, LENGTH = 128K
M7 .ld File
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1896K
I also make adjustments with cube programer as in the picture.

Core m7 works but m4 doesn't seem to work.I think I'm missing something or doing something wrong. Can you help me?
Codes are as follows
CM4 Main Code :
int main(void)
{
MPU_Config();
__HAL_RCC_HSEM_CLK_ENABLE();
HAL_HSEM_ActivateNotification(__HAL_HSEM_SEMID_TO_MASK(HSEM_ID_0));
HAL_PWREx_ClearPendingEvent();
HAL_PWREx_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFE, PWR_D2_DOMAIN);
__HAL_HSEM_CLEAR_FLAG(__HAL_HSEM_SEMID_TO_MASK(HSEM_ID_0));
HAL_Init();
MX_MDMA_Init();
MX_DMA_Init();
MX_GPIO_Init();
MX_SPI1_Init();
while (1)
{
HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_13);
HAL_Delay(100);
}
}
CM7 Main Code :
int main(void)
{
int32_t timeout;
MPU_Config();
SCB_EnableICache();
SCB_EnableDCache();
timeout = 0xFFFF;
while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0));
HAL_Init();
SystemClock_Config();
PeriphCommonClock_Config();
__HAL_RCC_HSEM_CLK_ENABLE();
HAL_HSEM_FastTake(HSEM_ID_0);
HAL_HSEM_Release(HSEM_ID_0,0);
timeout = 0xFFFF;
while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) == RESET) && (timeout-- > 0));
if ( timeout < 0 )
{
Error_Handler();
}
MX_GPIO_Init();
while (1)
{
HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_1);
HAL_Delay(100);
}
}