Question
STM32H7 faster using floats than using uint32_t
I made following two versions of the same software to process DMA data, one using floats and the second using uint32_t to try run faster, but as a surprise the first one run faster:
//161
void process_data_ADC1()
{
float samples1=(2.0f/(float)ADC_BUF1); // =1/samples
uint32_t media1=0,media2=0;
for (int i=0;i<ADC_BUF1/16;i++)
{
for (int j=0;j<8;j++)
{
media1+=buffer_ADC1[i*16+j];
media2+=buffer_ADC1[i*16+j+8];
}
}
float med1=(float) media1*samples1;
float med2=(float) media2*samples1;
avg16[1]=(uint16_t) (16.0f*med1+0.5f);
avg16[2]=(uint16_t) (16.0f*med2+0.5f);
float rms1=0.0f,rms2=0.0f,x;
for (int i=0;i<ADC_BUF1/16;i++)
{
for (int j=0;j<8;j++)
{
x=(buffer_ADC1[i*16+j] -med1);rms1+=x*x;//maximo 2^12 sin overflow para 12 bits
x=(buffer_ADC1[i*16+j+8]-med2);rms2+=x*x;
}
}
rms16[1]=(uint16_t) (16.0f*sqrt(rms1*samples1)+0.5f);
rms16[2]=(uint16_t) (16.0f*sqrt(rms2*samples1)+0.5f);
}
//161b Usando uints32 en vez de float: ES MAS LENTO!!!!!!!
void process_data_ADC1_fast()
{
float samples1=(2.0f/(float)ADC_BUF1); // =1/samples
uint32_t media1=0,media2=0,samples00=ADC_BUF1/2;
for (int i=0;i<ADC_BUF1/16;i++)
{
for (int j=0;j<8;j++)
{
media1+=buffer_ADC1[i*16+j];
media2+=buffer_ADC1[i*16+j+8];
}
}
float med1=(float) media1*samples1;
float med2=(float) media2*samples1;
avg16[1]=(uint16_t) (16.0f*med1+0.5f);
avg16[2]=(uint16_t) (16.0f*med2+0.5f);
media1=media1/samples00;media2=media2/samples00;
uint32_t rms1=0,rms2=0,x;
for (int i=0;i<ADC_BUF1/16;i++)
{
for (int j=0;j<8;j++)
{
x=(buffer_ADC1[i*16+j] -med1);rms1+=x*x;//maximo 2^12 sin overflow para adc de 12 bits y variables de 32 bits
x=(buffer_ADC1[i*16+j+8]-med2);rms2+=x*x;
}
}
x=16.0f*sqrt((float) rms1*samples1);rms16[1]= (uint16_t) (x+0.5f);
x=16.0f*sqrt((float) rms2*samples1);rms16[2]= (uint16_t) (x+0.5f);
}
This is the routine used to measure time:
uint32_t measure_time(void)
{
uint32_t static start = 0;
uint32_t time2= SysTick->VAL;
time2=start-time2;
//DELAY_US(10);
start=SysTick->VAL;;
return (time2);
}
(It surprised to me that the systick timer runs backward)
It took in debug mode:
49321 ticks the float routine
49321 tics the uint32_t routine