STM32H7 GPIO Default Behavior
Hi,
I notice in the STM32H747XIH6 reference manual (RM0399) that
"During and just after reset, the alternate functions are not active and most of the I/O ports
are configured in analog mode."
I want to confirm that in "analog mode" the IO is an HZ input without internal pullup or pull-down resistor enabled? Also, can anyone confirm which I/O ports do not assume this behavior on startup (since the RM says most)?
Thanks!