STM32H7 M7 to Update M4 flash area
Hello community!
I am developing an app that is running in an H7 MCU, the M7 core app is "turning on" the M4 and then is running to an external flash where is the actual M7 code.
I am looking to implement an update in this M7 "bootloader". As i understand, before "turning on" the M4, i can interact with the flash region where the M4 has its code to run, so my idea is in the M7 bootloader to start an USB port to detect an USB disk and if there is a .bin file for each core, to write the M7 in the external ram (using a code similar to the developed external loader for example?) and for the M4, just a write in the M4 memory location?
I look forward for your commends dear community :)
Thanks!