Skip to main content
Graduate
May 19, 2025
Solved

STM32H7 Timer Compare missed the first time

  • May 19, 2025
  • 3 replies
  • 644 views

I have an odd issue.  I am setting up a timer compare channel for a 5ms delay in the future.  I set the counter to 0, set the compare value to 5ms in the future.  The compare interrupt does not occur, until the timer wraps all the way around and passes the compare value for a second time.  It passes the compare value the first time with no interrupt.

Setup is:  STM32H753 (on custom HW), TIM2, Ch1/Ch2 used for PWM input capture. Ch3 used for timeout if IC does not occur.  All setup is using STM32Cube MX.  See code below.  The timers are started with the following code:

The idea is that the PWM input rising edge on Ch1 will reset the counter every cycle (1kHz), but if the counter does not get reset due to no PWM input signal for 5ms, Ch3 compare happens.  Everything works as expected except if there is no input signal from the start, the timeout takes a full timer roller over, instead of 5ms, then is always 5ms after that! 

It is like the timer needs to do a rollover first before output compare works.  I tried setting UG bit and CC3G bit in EGR, but did not help.  I even tried setting the counter to near rollover so it could roll over, but still didn't work!  I also tried removing all Ch1/2 functionality and disabling slave mode.  Just simple single channel as output compare.  Still same behavior!

Any help would be greatly appreciated.

 

My code to start the timers:

static TIM_HandleTypeDef* const cPWMMeasTimer = &htim2;
#define cPWMMeasRisingChannel TIM_CHANNEL_1
#define cPWMMeasFallingChannel TIM_CHANNEL_2
#define cPWMMeasTimeoutChannel TIM_CHANNEL_3
#define PWM_MEAS_TIMER_CLK_FREQ 240000000UL
#define NO_PWM_MEAS_TIMEOUT_MS 5u

...

// Start PWM measurement
__HAL_TIM_SET_COUNTER(cPWMMeasTimer, 0x0);
__HAL_TIM_SET_COMPARE(cPWMMeasTimer, cPWMMeasTimeoutChannel, (NO_PWM_MEAS_TIMEOUT_MS * PWM_MEAS_TIMER_CLK_FREQ) / 1000u);
HAL_TIM_OC_Start_IT(cPWMMeasTimer, cPWMMeasTimeoutChannel);
HAL_TIM_IC_Start_IT(cPWMMeasTimer, cPWMMeasRisingChannel);
HAL_TIM_IC_Start(cPWMMeasTimer, cPWMMeasFallingChannel);

STM32Cube MX generated code:

void MX_TIM2_Init(void)
{

 /* USER CODE BEGIN TIM2_Init 0 */

 /* USER CODE END TIM2_Init 0 */

 TIM_SlaveConfigTypeDef sSlaveConfig = {0};
 TIM_IC_InitTypeDef sConfigIC = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};

 /* USER CODE BEGIN TIM2_Init 1 */

 /* USER CODE END TIM2_Init 1 */
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 0;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 4294967295;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_OC_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_IC_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sSlaveConfig.SlaveMode = TIM_SLAVEMODE_RESET;
 sSlaveConfig.InputTrigger = TIM_TS_TI1FP1;
 sSlaveConfig.TriggerPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
 sSlaveConfig.TriggerPrescaler = TIM_ICPSC_DIV1;
 sSlaveConfig.TriggerFilter = 0;
 if (HAL_TIM_SlaveConfigSynchro(&htim2, &sSlaveConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
 sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
 sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;
 sConfigIC.ICFilter = 0;
 if (HAL_TIM_IC_ConfigChannel(&htim2, &sConfigIC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_FALLING;
 sConfigIC.ICSelection = TIM_ICSELECTION_INDIRECTTI;
 if (HAL_TIM_IC_ConfigChannel(&htim2, &sConfigIC, TIM_CHANNEL_2) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_TIMING;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM2_Init 2 */

 /* USER CODE END TIM2_Init 2 */

}

Timer registers after all initialization and starting channels:

ADunc1_0-1747616054370.png

 

 

 

    This topic has been closed for replies.
    Best answer by ADunc.1

    I don't know what to say.  I spent hours and hours trying to debug this yesterday.  This morning everything is working exactly as expected.  Only thing that has changed is I turned power off to the board overnight.  I know that seems odd and a reset should clear everything, but I have no other explanation!

    3 replies

    Super User
    May 19, 2025

    > I tried setting UG bit and CC3G bit in EGR, but did not help.

    Observe the TIM registers after doing this: if both TIMx_SR.CC3IF and TIMx_DIER.CC3IE are set, and this did not result in the expected CC3-related interrupt service routine being called (while taking into consideration that during single-stepping in debugger interrupts are usually suppressed by debugger, i.e. you have to confirm in debugger that both above flags are set and then let the program continue running), then there's something wrong in the interrupt invocation fabric: either relevant interrupts are disabled in NVIC, or things got lost somewhere in Cube/HAL.

    I'd suspect the latter and I'd write my own ISR, discarding whatever Cube/HAL is doing. I don't use Cube.

    JW

    ADunc.1AuthorAnswer
    Graduate
    May 19, 2025

    I don't know what to say.  I spent hours and hours trying to debug this yesterday.  This morning everything is working exactly as expected.  Only thing that has changed is I turned power off to the board overnight.  I know that seems odd and a reset should clear everything, but I have no other explanation!

    Super User
    May 19, 2025

    Thanks for coming back with the solution, however unsettlig it is.

    Please click on "Accept as solution" in that post so that the thread is marked as solved.

    JW

    ADunc.1Author
    Graduate
    May 19, 2025

    To be honest, I an skeptical, but what can I say, with zero code change it fixed itself overnight!!!