STM32H7 - UART DMA working only in debug mode
dear all, my STM32H7 based project implements three DMA streams, one for a SAI peripheral, a second one for the ADCs and the third one for UART comm.
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Stream0_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn);
/* DMA1_Stream1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);
/* DMA1_Stream2_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream2_IRQn);
}
What I have noticed is that the UART interface works only when in debug mode. SAI and ADC instead work fine. Do you have any idea about where should I investigate the issue ? Thanks