STM32H7 USB Audio as USB device class
Hi everyone,
in my latest PRJ, i had to run some arbitrary waveforms. The idea was to connect my STM32H7 to the host and configure it as USB audio device. As far as good...the problem is that i had to drive 60kSps (16Bit). So since i've read on the X-CUBE-USB-AUDIO description, that sampling rates up to 96kHz/24Bit are possible, but from the CUBE device configuration there is the limit to 48kHz.
Is this just a CubeMX thing and i can configure my USBD_AUDIO_FREQ to 60000?
Thank you!