STM32H7 won't calibrate using STMCubeMX v6.13.0
CubeMX-generated code gets stuck on HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED) using IDE v1.17.0 and FreeRTOS.
RTOS is using SystemCoreClock. HAL Tick is using TIM17 with a priority = 14 (Higher than SysTick Timer.)
Made AdcTask highest priority task. Ran ADC_Disable(&hadc1) to make sure ADC was disabled. All required GPIO Port Timers have been enabled. Not using DMA. I can't see any relevant difference between my code and the examples.
If I skip Calibration and then:
ADC_Enable(&hadc1);
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1, 10)
The ADC enables and starts, but times out at the Poll. This could be a different issue, but it may also be an indicator of why it wont calibrate. ADC is configure to Scan 4 channels with EOS.
All other GPIO, UART, I2C, Timers work as expected.
A response would be appreciated.