Skip to main content
Visitor II
November 18, 2025
Question

STM32H723 ADC Specification

  • November 18, 2025
  • 1 reply
  • 176 views

I am trying to measure DC output of an RF detector (AD8363) using STM32H723's ADC. The Signal that is to be measured has about 80 mV - 90 mV of high frequency noise embedded on it. Due to inaccuracies in the measurement I am probing the measurement circuitry and therefore would like to know:

  1. The 5 pF capacitance of ADC is total capacitance of the 12 or 16 capacitors inside ADC or just that of one capacitor?
  2. What is the resistance of the ADC's sample and hold switch?
  3. Is there any model of ADC Circuitry, that includes parasitic as well?
  4. What is the tracking bandwidth of the ADC?
    This topic has been closed for replies.

    1 reply

    Super User
    November 18, 2025

    These are listed in the datasheet.

    TDK_0-1763468957245.png

     

    RAIN and CADC form a low-pass filter as described:

    TDK_1-1763469026549.png

     

    SarmadAuthor
    Visitor II
    November 18, 2025

    Thanks for sharing that. I was going through AN2834, where a little detailed internal circuit of ADC is shared:

    Sarmad_0-1763470059548.png

    that lead me to query the datasheet specs. So is the CADC equivalent of all these capacitors or just the C. And what about tracking bandwidth?

    Explorer
    November 18, 2025

    Capacitance 5 pF total.

    Bandwidth is defined by first order LPF:  Fbw = 1/ 2 x PI() x Rin x Cin