stm32h723 can not connect to the targer by SWD
I am not new in using STM32H7 products but in my last project I can not connect the target by ST_Link.
I take care about power supply, pins to connect at GND or 3V3 and so on but the Link-Utility return this error:
<<
08:28:41 : ST-LINK SN : 440032001500004737364D4E
08:28:41 : V2J43S7
08:28:41 : Connected via SWD.
08:28:41 : SWD Frequency = 4,0 MHz.
08:28:41 : Connection mode : Normal.
08:28:42 : Can not connect to the target!
Please select "Connect Under Reset" mode from Target->Settings menu and try again.
08:28:53 : Unexpected error
>>
It seems the comunication start with the target but can not complete it.
I Try all possible combinations of the ST_Link Utility configurations not no results
Can anyone help me to solve this problem?
Is there a specific list of pin to connect at 3V3 or GND or with CAPS and so on in order to let the target comunicate properly.
Thanks for you support