STM32H723 Internal Temperature Measurement vs. Ambient
All:
Setup - STM32H723 with VREFP = 3.00 V
I have connected internal temperature to ADC3, and I am able to display degrees C on "Live Expressions". With VREFP set to 3.00 V, I am seeing lower readings than ambient. Using __HAL_ADC_CALC_TEMPERATURE( ), I am seeing internal temperatures of 21 - 24 C, vs. ambient temperature of 25.8 C.
Is there a variation based on VREFP? (Earlier on Nucleo board, I was seeing internal temperature of 30 C with VREFP of 3.3 volts.)
Regards,
Todd Anderson