STM32H723 - ULPI and pc2_c/pc3_c
Hi all,
I'm currently designing a board that requires using an stm32h723 with USB HS (I need more bandwidth than FS allows). The stm32h723 I'm using doesn't expose pc2 or pc3, which are needed for ULPI DIR and NXT respectively. Instead, pc2_c and pc3_c are exposed as pins on the chip. These are internally connected to pc2/pc3 internally with an analog switch, but is this really sufficient for ULPI? The datasheet doesn't seem to be clear.
The stm32h747 datasheet does specify using ULPI over pc2_c/pc3_c, which makes me think it's at least been considered. I'm curious why it doesn't seem to be specified in the stm32h723 datasheet (either specifying whether it will or won't work)
I did find a few forum posts of people using pc2_c/pc3_c with USB, although it seemed like this had issues (including hardware damage, possibly of the analog switch itself).
Thanks!