STM32H723 using DMA method to implement timer input capture can only be executed once?
Purpose: We would like to implement timer input capture in DMA mode on STM32H723 platform without interruption.
Current Problem: Use Cube MX to configure relevant parameters, only use CH2 of TIM4 as the direct mode for input capture, select Reset Mode for Slave Mode, select TI2FP2 as the trigger source, and then generate the corresponding code.
The frequency measurement works, but only once, if the external input frequency decreases from 1000Hz to 500Hz, it can only reset the programme to run at full speed again to measure 500Hz again, otherwise it will always be 1000Hz. not sure what the problem is? I suspect the trigger source may not be configured correctly? Or do you have to switch on both CH1 and CH2 channels, one directly and one indirectly? Please refer to the attached file for the configuration.
Any guidance would be greatly appreciated!
*This post has been translated from Chinese to comply with the ST Community guidelines.