Skip to main content
Visitor II
May 8, 2025
Question

STM32H723VGT6 DMA2 Controller Fails Silently After Prolonged Operation – No Error Flags Reported

  • May 8, 2025
  • 1 reply
  • 396 views

Problem Description:
MCU Model: STM32H723VGT6
DMA Configuration:

  • DMA1/DMA2 handles 15 DMA channels in total:
    • 5 UARTs (TX + RX)
    • 4 additional UART RX channels
    • 1 PWM channel (TIM15 CCR1 via DMA)
      Observed Failure:
      After 10–60 minutes of normal operation, ​all peripherals using DMA2 stop functioning:
  1. UARTs: RX overrun errors occur (ORE flag set in ISR).
  2. PWM (TIM15 CCR1):
    • DMA circular mode remains active (Half/Complete Transfer interrupts trigger normally).
    • SxNDTR counts correctly, but ​CCR1 register data never updates (verified via debugger).
  3. No DMA Error Flags:
    • TEIF (Transfer Error), FEIF (FIFO Error), and other error flags in DMA_LISR/HISR remain cleared.

Key Observations:

  • Failure ​suggests DMA2 loses access to data bus without triggering error detection mechanisms.
  • Issue persists across multiple boards, ruling out hardware defects.

Troubleshooting Performed:

  1. DMA buffer addresses confirmed in AXI SRAM (0x24000000) with MPU full-access permissions.
  2. Interrupt flags (TCIF, HTIF) cleared properly in ISRs.

Request:
Has anyone encountered similar DMA2 silent failures? Any insights into:

  • Potential AXI bus arbitration conflicts?
  • Hidden errata related to DMA2 bus access?
  • Debugging techniques to capture transient bus faults?

Thanks in advance for your expertise!

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    May 26, 2025

    Hello @peter_zhly and welcome to the community;

     

    Do you have the same issue when all USART are disabled?

    Could you please check if this errata is respected or not in your project code? 

    KDJEM1_0-1748253663816.png

    Thank you.

    Kaouthar