Skip to main content
Visitor II
September 30, 2025
Question

STM32H723VGT6 hardware error interrupt is occurring

  • September 30, 2025
  • 1 reply
  • 527 views

hi ;During the operation of STM32H723VGT6, the constant input bus error and hardware error interrupt occurred, and the clock is 280M. The PWR_REGULATOR_VOLTAGE_SCALE1 is unstable. The clock configuration __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0) was modified. The result is stable. Could you please help confirm what the reason isst ..................jpg

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    September 30, 2025

    Dear @leo12345678 ,

    can you let us know which clock is at 280MHz , CPU one of AXI Bus or AHB ?

    IMG_4500.jpeg

    A special care also to check with pins 48 and 73 that are connected to VCAP capacitor of 2.2uF having a Lower value may create such behavior .

    Hope it helps you .

    STOne-32