STM32H723ZG max ADC data transfer rate
Hi,
I'm confused about the maximum data transfer of the STM32H723ZG. The overview says:
- 2×16-bit ADC, up to 3.6 MSPS in 16-bit: up to 18 channels and 7.2 MSPS in double-interleaved mode
Then the 'AN5354 - Getting started with the STM32H7 Series MCU 16-bit ADC' also mentions these data rates for the H7 series but not specifically the STM32H723ZG. This application note also specifies a huge discrepancy between different packages and rates:

Then, assuming these numbers correspond to the direct channels, what are the data rates for the fast or even slow channels?
Also, CubeMX doesn't clearly indicate which ADC channels are direct, fast or slow, maybe this is a functionality that could be added?