STM32H723ZG Unable to connect to ST_LINK when powering on for the first time, and the COM port canno
Hello everyone:
After I got the development board, I soldered it first. After soldering it, only the COM port light lit up red when I powered on for the first time, and the LED area and user buttons did not respond. After using the debug support of keilv5, I successfully read the port. However, I cannot connect to the hardware when using keil's ST download function. I tried to use cubeide to download again, but the port still could not be found, but my computer device manager could find the port and the universal serial bus device could query STM32 ST-Link/V3. I have the following screenshots as a supplement.