Skip to main content
Graduate
April 29, 2025
Question

STM32H723ZGT6 USB_OTG_HS in FS Mode Not Detected by PC (No External Oscillator)

  • April 29, 2025
  • 4 replies
  • 1466 views

(Please see attached PDF for best formatting and screenshot images. Complete code of main.c and usbd_cdc_if.c are also attached as txt.)

Hi everyone, 

This is my first post! Please excuse any mistakes I might make in my question :).

Question & Problem Description:

I am trying to use the USB_OTG_HS functionality in Full Speed (FS) Mode on a custom STM32H723ZGT6 microcontroller custom PCB. However, the USB is not detected by any computer — nothing appears when I plug it in (no device, no "unknown/unrecognized USB" error, no activity at all).


I am using ST-Link/V2 for programming/debugging.

 

The Project so Far:

Successes of my Project:

I can get the LED in PA10 to blink with programmed interval (using a specific HAL_Delay() time), turn ON or turn OFF.

Problem of my Project:

I would like to be able to communicate with my computer to change the duration of blinking based on user input. I have divided this into 4 steps.

  1. Be able to blink LED without user input (just run the code and ensure everything is working). This is done and correct.

  2. Get the device to transmit “Hello World” message to the host computer and I should receive this message on my host computer. → I am unable to do this. My host computer does not even see the microcontoller PCB when I plug it in (It doesn’t even give a “USB not recognized” error – it just “does nothing”).

  3. Once steps 1 & 2 are working, I would like to give some command to the STM32H723ZGT6 microcontroller via terminal and then receive some response based on my input.

  4. Once 3 is working, I would like to submit the duration for the blink via terminal to the microcontroller, which will adopt the blinking interval based on my user input.

Setup Details:

Computers Used for Testing:

  • Linux (Ubuntu 24.04.2)

  • Windows 10

  • Windows 11 (different computer)

  • (Both show no device detected when the microcontroller is plugged in.)

 

Software Used for Programming: STCube IDE

Oscillator

 

No external oscillator is installed. According to the data sheet (https://www.st.com/resource/en/datasheet/stm32h723ve.pdf, pages 50/257 and 231/257), the internal HSI48 clock should be sufficient for FS mode.

Hardware (USB connection):

  • USB-C connector wired directly to PA11 (DM) and PA12 (DP).

  • No series resistors between DP/DN and the USB port.

  • Both DP and DN lines are protected with ESD protection diodes.

  • CC1 and CC2 are pulled down to GND with 5kΩ resistors (indicating a USB device, not a host).

  • PA10 is connected to an LED for testing.

PCB is Manufactured

PCB is already produced by JLCPCB so we need to stick to the current schematic/layout if possible.

See attached PDF for schematic.

Pin Configuration:

  • PA10: LED_Out pin (SET = ON; RESET=OFF)

  • PA11: USB-OTG_HS_DM

  • PA12: USB-OTG_HS_DP

  • PA13: DEBUG_JTMS-SWDIO

  • PA14: DEBUG_JTCK-SWCLK

  • All others are default.

Clock:

    • I clicked “Resolve Clock Issues” and now 48MHz to USB using HSI (even in the PLL Source Mux).

    • No errors are reported by the software.

See PDF for screenshots of my clock settings.

 

Other Configuration Settings:

    • RCC > High Speed Clock (HSE) > Disable

    • RCC > Low Speed Clock (LSE) > Disable

    • Connectivity > USB_OTG_HS > External Phy > Disable

    • Connectivity > USB_OTG_HS > Internal FS Phy > Device_Only

    • Connectivity > USB_OTG_HS > Active_SOF > Disable

    • Connectivity > USB_OTG_HS > Activate_VBUS > Disable [The reason this is disabled is because I did not connect anything to PA09, so I fear if I turned this on then the USB would never be on since it would never measure anything on VBUS (PA09).]

    • Middleware and Software Packs > USB_DEVICE > Class For HS IP > Communication Device Class (Virtual Port Com)

    • Trace and Debug > Debug > Serial Wire [I am using STLink/V2.]

Code:

    • Please see the full code attached as “main.c” and “usbd_cdc_if.c” files

    • Specific changes that I made are:

main.c: (See attached complete main.c file)

    • including usbd_cdc_if.h file in line 25:

      • #include "usbd_cdc_if.h"

    • making a USB transfer buffer with known size to transferring in lines 46-47:

      • uint8_t usbTxBuf[USB_BUFLEN]; /* We need a measure of the length of the Tx buffer*/

      • uint16_t usbTxBufLen;

    • Printing the transfer details line 118-121:

      • usbTxBufLen = snprintf((char *) usbTxBuf, USB_BUFLEN, "%lu\r\n", HAL_GetTick()); /* */

      • CDC_Transmit_HS(usbTxBuf, usbTxBufLen);

      • HAL_Delay(500); /* Send the text every 500 ms*/

usbd_cdc_if.c: (See attached complete usbd_cdc_if.c file)

    • Specified the baud rate, number of bits and some details in lines 98-103:

      • USBD_CDC_LineCodingTypeDef LineCoding = {

        • 115200, /* baud rate */

        • 0x00, /* stop bits - 1 */

        • 0x00, /* parity - none */

        • 0x08 /* nb. of bits 8 */

      • };

    • CDC_SET_LINE CODING in lines 230-235:

      • case CDC_SET_LINE_CODING:

        • LineCoding.bitrate = (uint32_t) (pbuf[0] | (pbuf[1] << 8) | (pbuf[2] << 16) | (pbuf[3] << 24));

        • LineCoding.format = pbuf[4];

        • LineCoding.paritytype = pbuf[5];

        • LineCoding.datatype = pbuf[6];

        • break;

    • CDC_GET_LINE_CODING in lines 237-245

      • case CDC_GET_LINE_CODING:

        • pbuf[0] = (uint8_t) (LineCoding.bitrate);

        • pbuf[1] = (uint8_t) (LineCoding.bitrate >> 8);

        • pbuf[2] = (uint8_t) (LineCoding.bitrate >> 16);

        • pbuf[3] = (uint8_t) (LineCoding.bitrate >> 24);

        • pbuf[4] = LineCoding.format;

        • pbuf[5] = LineCoding.paritytype;

        • pbuf[6] = LineCoding.datatype;

        • break;

 

 

    This topic has been closed for replies.

    4 replies

    Super User
    April 29, 2025

    > However, the USB is not detected by any computer — nothing appears when I plug it in (no device, no "unknown/unrecognized USB" error, no activity at all).

    This suggests the device isn't pulling up the USB data lines at all. Try a different cable and port. Ensure you're not using a power-only cable.

    Try holding BOOT0 high during reset to connect to the internal USB DFU bootloader.

    Try downloading a CubeMX example which uses the USB and see if that works.

    sga2Author
    Graduate
    April 29, 2025

    Hi,

    Thank you so much for your quick response.

    1 - I changed USB cables as well. I believe they both had data transfer lines because when I plug my phone into my computer via these cables, I can access my phone's internal shared storage and file transfer between the phone and my computer. That implies data transfer capabilities, correct?
    2 - I'm not sure what you mean? Should I disconnect BOOT0 from the STLink/v2, connect it to +3.3V and then upload the program via STlink/V2?
    3 - I tried searching for an example that doesn't have an external oscillator for STM32H but could not find one. If you know one, can you please suggest?

    Once again, thank you for your quick response.

    SGA

    Super User
    April 29, 2025

    Where are your capacitors for VCAP? Why is PDR_ON floating?

    TDK_0-1745947297569.png

    Getting started with STM32H723/733, STM32H725/735 and STM32H730 Value Line hardware development -

     

    > I'm not sure what you mean? Should I disconnect BOOT0 from the STLink/v2, connect it to +3.3V and then upload the program via STlink/V2?

    BOOT0 isn't connected to the programmer. Read AN2606 for ways to boot into the bootloader.

    STM32 microcontroller system memory boot mode - Application note

     

    > I tried searching for an example that doesn't have an external oscillator for STM32H but could not find one. If you know one, can you please suggest?

    This example uses HSE bypass, which is an 8 MHz signal from the st-link's HSI.

    STM32CubeH7/Projects/NUCLEO-H723ZG/Applications/USB_Device/HID_Standalone/Core/Src/main.c at master · STMicroelectronics/STM32CubeH7

    sga2Author
    Graduate
    May 6, 2025

    Hi TDK,

    Thank you for your answer.
    Floating/Missing Pins

    So actually they aren't actually floating, I just removed them to better highlight the  situation. I've attached the actual schematic here to avoid confusion.

    BOOT0
    Thank you! I think I understand what you mean. Do you mean that the BOOT0 is only used to start the bootloader?

    Your Provided Example:

    I will try it and let you know! Thank you!

    Thanks,

    SGA

    Technical Moderator
    April 30, 2025

    hello @sga2 

    I have attached a working project for the CDC class, featuring both receive and transmit functions on an H723ZG board. This project includes the IOC configuration and the functions used, which should help you determine whether the issue lies with the hardware or software. Please review the attached files and let me know if you need further assistance.

    sga2Author
    Graduate
    May 6, 2025

    Hi Gyessine,

    Thank you for sending this! This is perfect! I will try it and then update you.

    Thanks,

    SGA