Skip to main content
Visitor II
August 5, 2025
Solved

STM32H725VGT3TR Vref changes when I enable ADC1

  • August 5, 2025
  • 4 replies
  • 233 views

I have my internal Vref set to 2.5V (stage 0).  

RallyTronics_1-1754427522996.png

The value reads correct (2.52V) with a meter on the test point below until I call HAL_ADC_Start_DMA().   Once HAL_ADC_Start_DMA() -> ADC_Enable() -> LL_ADC_Enable() is called the voltage goes up to around 2.9V.

 

RallyTronics_0-1754427194978.png

Any thoughts as to why this is happening?

 

Thanks!

    This topic has been closed for replies.
    Best answer by TDK

    Are you converting channels out of bounds? (above 2.5 V?)

    4 replies

    TDKAnswer
    Super User
    August 5, 2025

    Are you converting channels out of bounds? (above 2.5 V?)

    Visitor II
    August 5, 2025

    No, I am currently trying to digitize a 1V DC test signal.

    Visitor II
    August 5, 2025

    Let me double check my unused channels.

    Visitor II
    August 5, 2025

    Looks like that's the problem.