STM32H730 outside of program code
Hello!
I'm porting a working code from H750VB to H730VB, generating a new HAL core from STM32CubeMX, but right after entering on "SystemClock_Config" function at debug mode, I've got the message "Break at address 0x46bd3718 with no debug information available, or outside of program code". Going step-by-step, the issue happens on "HAL_RCC_ClockConfig", at the second "D1PCLK1 configuration" calling:
if ((RCC_ClkInitStruct->APB3CLKDivider) < (RCC->D1CFGR & RCC_D1CFGR_D1PPRE))
{
assert_param(IS_RCC_D1PCLK1(RCC_ClkInitStruct->APB3CLKDivider));
MODIFY_REG(RCC->D1CFGR, RCC_D1CFGR_D1PPRE, RCC_ClkInitStruct->APB3CLKDivider);
}
I'm using the same custom board and pinout as H750 one and the app is quite simple: a few GPIOs, UART and SPI. I've also tried just a "blink LED" code, same break on "SystemClock_Config". Two different boards, same issue.
Did anyone face the same problem?
Thanks!