STM32H730VBxx: no OCTOSPIM registers
A question of compehension:
I cannot find any of the OCTOSPIM registers - neither in STM32CubeMX, nor in the register list, read by STM32CubeProgrammer. Am I right, that's because in our chip, there's only one OCTOSPIM port?
(I would appreciate, if that was mentioned in the reference manual, that that whole section "OCTOSPI I/O manager (OCTOSPIM)" has no relevance for certain chip subtypes, with a reference to the data sheet.)
But then I ask: Why do I still have the OCTOSPI2 registers? Because "In the default out-of-reset configuration, all the OCTOSPI1 and OCTOSPI2 signals are mapped, respectively, on Port 1 and on Port 2." (reference manual). And since I cannot change that mapping, and since I have no OCTOSPIM2 port, what's the point in the OCTOSPI2 registers then?
Did I misunderstand / miss something?